Part Number: TPS25810-Q1
Other Parts Discussed in Thread: TPS25810
Hi,
My customer is worrying about current limit value.
The load(mobile battery) of their system requires 2.1A(max).
So they must select 3.4A(typ) to current limit value of TPS25810.
However we consider that current limit value is too large than actual maxim current.
Do you thiink that this current limit setting is appropriate?
Or should they locate another current limit power SW?
Best Regards,
Kuramochi