Part Number: DS90LV804
Hi Sirs,
As title, we have some questions on DS90LV804
1. When will use the Output Interfacing?
2. Does DS90LV804 had double termination recover plan? if yes the default is open?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90LV804
Hi Sirs,
As title, we have some questions on DS90LV804
1. When will use the Output Interfacing?
2. Does DS90LV804 had double termination recover plan? if yes the default is open?
Greetings -
The DS90LV804 should be treated like most LVDS devices. The output expects to drive a single load with a 100 ohm resistive termination. The internal 100 ohm termination in the DS90LV804 output structure is there to indicate that the device has a 100 ohm resistance internally.
This interface is shown in your attached graphic.
2. There is no need to externally terminate the DS90LV804 at the output pins.
Best Regards,
Lee