This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH940-Q1: MIPI display interface

Part Number: DS90UH940-Q1

Hello,

We are trying to use a Processor that has MIPI DSI interface or HDMI interface to connect to a display. We have also identified a display(1080p 30fps) which supports MIPI DSI.

As per the Display Serdes page of ti, http://www.ti.com/interface/fpd-link-serdes/display-serdes/overview.html i can use 949A/949 for Processor (HDMI-->fpdlink) and 940A/949 for Display(fpdlink --> MIPI CSI).

My questions is: MY display supports MIPI DSI input. It the above link it is mentioned that 940 device output is MIPI CSI.