Part Number: TUSB211
Hi Team,
Customer designs TUSB211 on the host application
Customer do the experiemnt with and w/o TUSB211.
Could you please provide your comment why the USB2.0 device sometimes fail with TUSB211?
Experiment:
Customer tested without TUSB211 USB Conditioner for 10 cycles :
With TUSB211: pass x6, fail x4 (the test result is below)
Without TUSB211: pass x10, fail x0
Pass scenario, D- high level is normal (3V) and we can see low pulse by HOST perform reset, keyboard is functional

Fail scenario, D- high level is around 1V, keyboard is not functional.
After re-plugging USB cable, then D- will become to normal (3V), then HOST can perform reset and keyboard is functional
Thanks,
SHH