Part Number: SN75182
I have a problem with the SN75182 line receiver. In general, the circuit works and the received messages at the output pin 6 are OK . But after a few weeks, the circuit is defect and I have to replace it by a new one. This happened the 4. time.
Pin 1 and 3 are connected to the RS485 lines. Between pin 2 (RT) and pin 1 a 3,3 nF capacitor is connected. Pin 4 (STRB) and pin 14 are connected to +5V. Pin 6, the TTL output is connected to the RxD of an Microprocessor. Pin 7 is connected to ground. All other pins are not connected. I assume the problem at the input side of the chip, not at the TTL output.
What could be wrong with my design ?
Lorenz