This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1046A-DCI: Rx AC Coupling Capacitors for TUSB1046A-DCI

Guru 29720 points

Part Number: TUSB1046A-DCI

Hi Team,

I believe Rx AC Coupling Capacitors are required for TUSB1046A-DCI because of the following E2E thread.
Is it correct?
https://e2e.ti.com/support/interface/usb/f/1008/p/639091/2358806#2358806

If the answer is yes, I would also like to know the recommended capacitor value.
Is it same value as TX (75~265nF)?

Best Regards,
Yaita / Japan disty