Part Number: TPS65982
Hello,
I have an application which is essentially a dock. The dock is self-powered, and it is able to provide power for charging the device connected to the UFP. It is primarily battery-powered, and when it is using battery power, it can only supply limited or no power for charging the upstream device. However, when it is connected to an AC power source, it is able to provide power for charging the upstream device. I believe I can accomplish this with the tps65982, but when I run the configuration tool I'm not sure which prototype project to select. I believe it would be DRP_Source_Advanced? The descriptions for that and DRP_Source_Standard are the same, so I'm not sure what the differences are. Basically I'm a powered hub that can sometimes, but not always, provide power for charging the upstream device. I don't need to support alternate modes at all, and I'll always be a UFP.
I would appreciate any advice you can give.
Thanks,
Tony