Hello,
I have a problem with the TUSB3410.
In this design, the TUSB3410 is connected to port 2 of a 7-port USB hub whose upstream port is connected to the USB 2.0 host port of a computer.
Device Manager (under Windows 7 and 10) both indicate there is a problem with the device.
The same design has worked in the past but directly connected to the USB 2.0 host port.
Can the TUSB3410 function when plugged into a USB 2.0 hub?