Part Number: TIC12400
HI team, Could I connect 2 inputs each sourcing 15mA to give 30mA capability?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi as a follow up question on teh ADC
I have a technical question with regards to the TIC12400…. You mentioned before that the ADC measures voltages from 0-6V (1024 max codes), but in the data sheet it mentions a VS Ratio bit that can be applied to increase the voltage measurement to 30Vdc – is this only for measuring the VS supply or can it be applied to the input monitor pins as well?