Part Number: DP83867IR
Hi all,
i am working on a system that requires clock synchronization over Ethernet. On the receiver side i think this task is easy to achieve - i am going to use the "CLK_OUT"-Pin to output the recovered receive clock. On the transmitter side i am not sure how the PHY works. Is the transmitter clock derived from the "TX_CLK" Signal as it is part of the RGMII Interface (Option A)? Or is the transmitter clock derived from the "XI" Input (Option B)?
If option A is the case i can use a simple free-running crystal to provide the "XI" Signal. For Option B i can't use a crystal for XI. Instead i have to provide a clock which is derived from other clocks in the system.
Best Regards
Michael