Part Number: TUSB422
Other Parts Discussed in Thread: MSP432WARE
Hi,
I have TUSB422EVM and MSP432P401R launcpad, and I want to launch sample code for this EVM on launcPad.
First i try to import sample code to CCS and launch, but with no luck. There is problem with tcpm_hal.c in function SystemInit which is called after Reset interrupt. CPU goes to Hardfault irq when trying to initialize Port J pins, which is needed for crystal.
Else i open project with IAR. And get the same result.
Function where i get HARDFAULT:
void GPIO_setAsPeripheralModuleFunctionInputPin(uint_fast8_t selectedPort,
uint_fast16_t selectedPins, uint_fast8_t mode)
{
uint32_t baseAddress = GPIO_PORT_TO_BASE[selectedPort];
HWREG16(baseAddress + OFS_LIB_PADIR) &= ~selectedPins; // There cpu crashes.
switch (mode)
{
case GPIO_PRIMARY_MODULE_FUNCTION:
HWREG16(baseAddress + OFS_LIB_PASEL0) |= selectedPins;
HWREG16(baseAddress + OFS_LIB_PASEL1) &= ~selectedPins;
break;
case GPIO_SECONDARY_MODULE_FUNCTION:
HWREG16(baseAddress + OFS_LIB_PASEL0) &= ~selectedPins;
HWREG16(baseAddress + OFS_LIB_PASEL1) |= selectedPins;
break;
case GPIO_TERTIARY_MODULE_FUNCTION:
HWREG16(baseAddress + OFS_LIB_PASEL0) |= selectedPins;
HWREG16(baseAddress + OFS_LIB_PASEL1) |= selectedPins;
break;
}
}
What am I doing wrong? please help.