Part Number: TPD2S703-Q1
Hi,
I would like you to confirm about below.
* According to datasheet of TPD2S703-Q1, there is following spec.
I believe that this capacitor is for :
1. To reduce noise superimposed on power supply.
2. To supply stable power even if the load fluctuates.
Then I have following question.
Q1. Could you please confirm whether above two understanding for Cvpwr is correct ?
Q2. If this understanding is correct, could you please tell me why you describe "min" value for this capacitor value ?
Customer asked us if Cvpwr value is less than 1uF (due to temperature variation), what is happen.
According to note of datasheet, since there is following description, user need to set over 1uF including capacitor error. However, if the purpose of this capacitor is above two, we can not understand why "min" value is required...
"Minimum and maximum values listed are inclusive of manufacturing tolerances, voltage derating, board capacitance, and temperature variation."
Best Regards,