Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84-Q1: Tolerance for I2C pins

Part Number: SN65DSI84-Q1

Hi,

I would like you to confirm about below.

* When power supply is NOT supplied to SN65DSI84-Q1 but 1.8V signal is applied for I2C pins, is there possiblity that device will receive damage ?

Here is my understanding.

According to dataheet, I understand that there is no possiblity that device will receive damage for "SCL".
1. Absolute voltage is defined fixed voltage (Not related to Vcc)
2. "SCL" has only "I"(CMOS input) function.


However, I'm not sure for SDA.
Because this pin has I/O function and output is defined as "Open-Drain".

So, I would like you to confirm about above.

Best Regards,