Part Number: DS90UB914A-Q1
Hello Sirs,
May I know if the high speed probe already have internal 50 ohm termination. Should I still place 100 ohm in CMLOUT+/- pin ?
Many thanks !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB914A-Q1
Hello Sirs,
May I know if the high speed probe already have internal 50 ohm termination. Should I still place 100 ohm in CMLOUT+/- pin ?
Many thanks !
Hi,
Are you using a Passive probe with 50Ohm Termination?
We suggest using a differential probe to monitor CMLOUT which would require the 100 Ohm termination between CMLOUT+/- pins.
It is possible to use a passive probe if you can supply a 50Ohm load to GND for each output, and use either output single-ended.
Sincerely,
Charley Cai
Hello Charley,
We use differential probe .So we always need external 100 ohm between CMLOUT+/- ,right ?
The reason why we ask this qyestion is differential probe have internal 50 ohm termination. We confused whether still need external 100 ohm or not,
And we remove 100 ohm the eye's height will bigger than populated 100 ohm.
TKS!