Part Number: HD3SS3220
Other Parts Discussed in Thread: TUSB320
1. In the data sheet it states : "HD3SS3220 mux does not provide common mode biasing for the channel. Therefore it is required that the device is biased from either side for all active channels. Also note that mux channels are for differential SS signals only. "
Where can I get information on this "common mode biasing for the channel" and "required that the device is biased from either side for all active channels"
2. FOR THE TUSB320 device : I just found this in the data sheets "If VBUS is guaranteed to be less than 5.5 V, powering the TUSB320 device
through a diode can be implemented" - my device is to be a UFP so the VBUS will be dependant on the PC \ Laptop USB port that I am connecting to - thus how can I guarantee that the VBUS will be less than 5.5V ?