Part Number: DS90UB913A-Q1
Other Parts Discussed in Thread: CDCE813-Q1
Hi TI,
My customer want to use the device under a repeater mode(like 925/926).
The connection is as below ;
(Camera)DS90UB913A ---> DS90UB914A ==> DS90UB913A ---> DS90UB914A(Navi)
Note ; ---> : Cable comnection
==> : parallel connection
Is it possible to use 913A/914A as repeater mode same with DS90UB925/926 ?
My concerns are:
1. The output jitter of DS90UB914A is too huge to use PCLK of DS90UB913A.
2. Does the I2C connection work between Navi(host) and Camera ?
3. Are there jitter cleaner needed at the parallel connection ?
How about the CDCE813-Q1 ? Is it work as a jitter cleaner for PCLK of DS90UB913A ?
Please let me know the possibility of the repeater mode ?