Part Number: PCA9557
Hi dear supporting team,
I heard there is a bug on PCA9557 , and it is revised on TCA9557, may I know what the bug is?
and are these two chips fully pin2pin compatible?
Customer found PCA9557 has very high requirement on POR, from d/s, if the residual voltage is lower than 0.2V than it can be POR sucessfully, so just double confirm with you, if the residual voltage is 0.1V, could the POR work normally?
and for the reset pin, could it work well to reset the internal stae machine?
tks a lot!