This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: DS90UB960-Q1 maximum serial bit rate

Part Number: DS90UB960-Q1

Hello guys,

I would like to know what is the maximum speed one can achieve with DS90UB960-Q1 deserializer?

I know there are 4 CSI-2 lanes each with maximum data rate of 1.6Gbps. This means 6.4Gbps of maximum speed per CSI-2 output port. Correct ?

I read in a datasheet that additional MIPI CSI-2 output port is available to provide additional bandwidth. What is the maximum speed we can have when using the second MIPI CSI-2 output?

In my design, I need to transfer data of 4 cameras. Each camera gives full HD image (1920x1080p) at 60Hz frame rate.

If I have 24-bits of data per pixel, data rate per camera would be: 2Mpx * 24 bits/px * 60images/s = 2.88Gbps.

For 4 cameras, data rate would be 2.88Gbps * 4 = 11.52Gbps.

Are my calculations OK or I'm missing something?

Is it possible to transfer that amount of data (11.52Gbps) with DS90UB960-Q1 module ?

Thank you very much for your time and effort.

Sincerely,

Bojan.

  • Yes, the DS90UB960-Q1 typically can support full HD at 60fps for 4 cameras. The DS90UB960-Q1 can support output data rates up to max rate of 6.656Gbps.Please note the CSI-2 data rate from different image sensors can vary for full HD depending on number of exposures or bits/pixel.
    The CSI-2 protocol also has some overhead based on the framing and packetization of the data.
  • Dear Liam,

    Thank you very much for your explanations. I would though need some confirmations and additional explanations...

    I am aware of the fact that different image sensors can have different CSI-2 data rate.

    When you say that DS90UB960-Q1 can typically support full HD at 60fps for 4 cameras, do you mean that two CSI-2 outputs (4 Lanes each) should be used to support this? If one CSI-2 output can support up to 6.656Gbps two can support up to 13.312Gbps. Correct?

    If image sensor gives 24-bits per pixes, for 1920 x 1080 px image, for 4 cameras, we would need the following rate (not counting the overhead):

    1920x1080 px * 24b/px * 60f/s * 4 cameras = 11.95Gpbs

    I'm afraid that if we count the overhead for framing and packetization of data, we will go beyound 13.321Gbps that we can have with two CSI-2 output.

    Are my calculations OK or I'm missing something?

    Can you recomend me some image sensors that can give me full HD image?

    Thanks once again.

    Sincerely,

    Bojan.

  • On the other hand, if I have full HD image (1920 x 1020), the same frame rate of 60fps but 8-bits per pixel, and having in mind the overhead, I believe it will be possible to deserialize 4 cameras with just one CSI-2 MIPI output (using all 4 lanes). Correct ?
  • Hi Bojan,

    your calculations are correct. So you can use each CSI-2 output for two Full-HD cameras.

    if you use the 8-bit or 12-bit resolution then you can have all 4 cameras on one CSI-2 output.

  • Hello Hamzeh,

    Thanks for your reply.

    I'm afraid of overhead.

    Two MIPI CSI-2 output ports can support 2 x 6.656Gbps = 13.312Gbps

    My data rate for 4 cameras without overhead for packetization and framing included is 11.95Gbps

    I'm afraid if we add the overhead to 11.95Gbps, we will be beyound 13.312Gbps. What is the amount of overhead I should take into consideration ?

    Thanks in advance.

    Sincerely,

    Bojan.

  • Hello Bojan,

    You are right; you need to calculate the imager data rate including the blanking period. The blanking is usually between 15% to 30%.
    So if I calculate your example we will have data rate of the imager = 1920 x 1080 x 24 x 60 x 1.2 = 3,583 Gbps which is not supported by the Serializer (953).
    So here you need to reduce either the blanking or the number of bits/pixel or number of fps.
    You need to get this number to max. 3,2 Gbps. if you have this number for 4 cameras then the Deserializer can support that without worry about the overhead, because it is already included in the blanking period.
  • Hello Hamzeh,

    Thank you for your explanations. 

    What is 1.2 in your calculation? Is it 20% of the blanking ?

    Concerning the blanking (that is usually between 15% and 30%), is it something that the user can set during the configuration?

    If I understand you well, I should not get over 3.2Gbps when I multiply: Image size * bits per pixel * frames per second * blanking. Please confirm. 

    Sincerely,

    Bojan.

  • Hi Hamzeh,

    would you mind to quickly address my questions ?

    Thanks in advance,
    Bojan.
  • 1.2 is 20% coding overhead (Fpdlink coding overhead). Ds90ub960 can support upto 4Gbps, raw data rate on each receive port