Other Parts Discussed in Thread: TUSB8041
Hi team,
My customer wants to know TUSB9261 absolute maximum ratings of IO(I,O,I/O) terminals.
I couldn't find these values on the datasheet.
I think these values are the same as TUSB8041.
Is the following description correct? Please let me know.
<< TUSB9261 absolute maximum ratings of IO(I,O,I/O) terminals >>
・USB_SSTXP,USB_SSTXM,USB_SSRXP,USB_SSRXM:
min -0.3V
max 1.4V
・XI:
min -0.3V
max 2.45V
・All other IO terminals:
min -0.3V
max 3.8V
Best regards,
Fumio Nakano