Part Number: DS90UB964-Q1EVM
Other Parts Discussed in Thread: DS90UB913A-Q1,
Hi,
I am using 964evm and 913, and an image sensor.
There are CRC errors with the reg 0xc and 0xa of 913.
Can anyone help me with this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB964-Q1EVM
Other Parts Discussed in Thread: DS90UB913A-Q1,
Hi,
I am using 964evm and 913, and an image sensor.
There are CRC errors with the reg 0xc and 0xa of 913.
Can anyone help me with this?
Hi,
1. For CRC, please reset it after power-on, then check the CRC counter register again;
2. please refer to page23 in UB964 user guide http://www.ti.com/lit/ug/snlu177/snlu177.pdf. as you use YUB422_8_8, the register 0x70 should be set 0x1E based on MIPI spec., while in our example, the 0x70 is assigned as 0x1F for 10bits mode.
best regards,
Steven
Hi Steven,
Thank you !
1. Use another cable, the crc error gone.
2. The image sensor and DS90UB913A-Q1 are provided by a third supplier. They said they have tested the 913 with 914 successfully. The mode they used was RAW12 HF.
I am testing it with DS90UB964-Q1EVM, but the LINE_LEN is not correct as I said before. Can you give me some suggestion?
Thanks!
Best Regards,
JT