Part Number: HD3SS215
Other Parts Discussed in Thread: TS3DDR4000
Hi,
1. can I use the device also for switching single ended lines and not just differential? (on the DA,DB lines). if yes, will they interfere to one onother (cross talk).
2. what is the bandwidth of such signals?
3. In general I need to mux 1:2 of 10 differential signals about 500MHz (so I want BW of at least 2.5GHz) , and 7 single ended signals at about 125MHz (so I want BW of at least 625MHz). will 3 devices do the job? (two devices each 4 diff (DA/DB) and 2 s.e in the AUX, and one with 2 diff (DA/DB) and 3 s.e in the aux or unused DA/DB.
thanks