Part Number: TPS65981
Other Parts Discussed in Thread: HD3SS460,
Some questions on handling the USB data lines. In the TPS6598x documentation, the USB data lines (D+ and D-) are routed through the chip and if USB 3.0 is needed then the two additional high speed diff pair lanes are routed through the HD3SS460 mux.
In some competing chips, the D+ and D- lines are not routed through the chip and it lets the connector handle the swap because of the way it got pinned out.
Do the TPS6598x chips need to have the D+ and D- lines routed through the chip? Is this so that the chip can interrogate the device\cable plugged in?
Similar question for the HD3SS460 mux, why can't the connector handle the connection swap?
I don't need the Display port, is there a smaller mux available to handle a non-display application?