Part Number: TUSB3410
HI team,
I know there is an 8052 MCU inside the TUSB3410.
I checked the reset block diagram and knew that the WDT reset connect with Reset Pin.
And WDT is supposed to be used basically.
I have a few questions below.
1. What code is in the 8052 in the new product?
2. Can I use the 8052 without entering the source?
3. Does using the default source cause continuous WDTs?
4. Can you provide a driver for Linux?