Part Number: TUSB1046EVM
Other Parts Discussed in Thread: TPS65986EVM, HD3SS460
Dear all.
USB3.0 device is not detected.during the TUSB1046 EVM test.
Test condition is
- EVM DP port : Signal generation
- EVM USB port : Notebook
- EVM Type-C port : 4k resolution monitor with Type C cable
- Connect the USB3.0 memory to the USB 3.0 port on the monitor.
As changed by GPIO configuration control in DS table 2, Notebook is confirmed to be connected to USB2.0 hub.
Changing another register is the same result.
Is there any way to make it look recognized as USB3.0? or should I use another device?
Thanks.