Part Number: TCA9617B
Hello,
I would use the IC for a 1-Wire BUS. I have the same configuration like on page 15 figure 13. Instead of I2C, I would have one 1-Wire. I would use the line SDAA and SCLA has no function. I think, I have a maximum speed of 1MHz.
1. Do you see any problems or have an alternative ideas?
2. In the datasheet on page 9: The SCL and SDA lines shall be at high-impedance when either one of the supplies is powered off.
This means, I get a problem, if VCCA has 0V, but the VCC at the pull up resistor has already 5V. Is it correct?
Thank you and best regards,
Dirk Seidel