This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS64MB201: Data Transmission Error from SIA to DOUT

Part Number: DS64MB201
Other Parts Discussed in Thread: DS125MB203

Hi, Team

My telecom customer is using DS64MB201 in their base station project. The DS64MB201 is used to switch the PCIe Gen-2 signal.

Customer find that the signal output from DOUT0+/- pins is different from signal input to SIA0+/- pins. There will be error in DOUT when there is continuously 0 or 1 in SIA.

Here is the signal waveform.

Pink: Signal input to SIA0+/-

Green: Signal output from DOUT0+/-

Is there any suggestion to solve the issue?

Thanks

Kevin Zhang