This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65981: MRESET and RESETZ pin behaviour

Part Number: TPS65981

Hi,

We have our make TPS65981 boards. We tied the MRESET pin to ground through 1MOhm as we're not using it in the application. With this state, the RESETZ pin state should be high always as mentioned in datasheet.

However, we observed the RESETZ pin state always logic LOW. During power-up, it is HIGH for few ns. Could you elaborate why the RESETZ pin state is not HIGH always?

Got to know that the MRESET pin active state can be configured in application code. We have used standard TI project template for flashing our application profile. Below I have attached the working project file FYR. TIIU_MMB1 TPS65981 HD3SS460 UFP Only 20171129.pjt

Regards,

Manikandan