Part Number: TPS65981
Hi,
We have our TPS65981 make boards and flashed the application image to it. Below is our application information.
Our application is 5V/2A sink which intends to pass power from VBUS to PPHV when standard USB-C PD complaint sourcing device is connected. So we tied BUSPOWERZ to 3.3V to disable the 5V pass to PPHV unless PD negotiates 5V/2A from the source.
When connecting NuPower PD adapter, we got 5V pass-through on PPHV, but not always. We're not seeing 5V output on PPHV during continuous plug/unplug. With Pixel Phone Charging Adapter also, the behaviour is same. Captured snaps in debug mode are here. With NuPower Adapter.zipWith Pixel Phone Adapter.zip
Regards,
Manikandan