Part Number: DP83849I
Hello,
So far I used DP83849I with a commercial crystal oscillator (0°C ... +70°C), but now I need higher temperatures so will use an oscillator in the industrial range (-40°C ... +85°C).
The crystal oscillator’s dimensions are 3.2mm x 2.5mm and it seems to be small so with a limited maximum power and it might need a series resistance on X2 (output).
In order to size all the resonant circuit and evaluate the gain margin I would like to know:
- Transconductance’s value of the amplifier used for the oscillator
- The parasitic capacitance across the pins X1 and X2 (The ds only provides 8pF for pin CMOS, but may be pins X1 and X2 might be different?)
Many Thanks,
Fax