Part Number: DP83822H
Other Parts Discussed in Thread: TLK105L, TLK105
The TLK105l supports an Isolation modus:
“When in the MII-Isolate mode, the TLK10xL … presents a high impedance on the TX_CLK, RX_CLK, RX_DV, RX_ER, RXD[3:0], COL, and CRS
otputs.”
The isolation modus is also active if a HW reset is applied to the PHY.
DP83822:
The Datasheet from the DP83822 says: “The DP83822 is a feature rich and pin-to-pin upgradeable option for the TLK105, …”
But the datasheet of the DP83822dosent does not say that it has an isolation modus which is activated at a HW reset.
Do the DP83822 have the same isolation modus like the TLK105l?