This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding 8 Port gigabit support chip controller

Hello Sir,

Can you suggest 8 GIGA BIT port ,IEEE 1588 PTP protocol supported chip controller 

  • Hi Denish,

    We do not offer a discrete, stand alone 8 port controller/switch. We only have integrated processor/switch devices like the Keystone II line of processors.

    Best Regards,
  • Hello Rob,

    Yes definitely this not possible, but mr. rob i just want, you suggest some chip controller / Processor which can fulfill bellow requirements so we can develop this product

    Requirement for MAC controller/Processor which support bellow requirements

    - MAC chip controller/processor support 8 giga speed port minimum. 

    -it should be UNMANAGE  switch controller

    -It support IEEE 1588 PTP Protocol supported 

    So dear Rob i want MAC device(Chip controller/processor) for develop this device not discreet components.