This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261: Choosing an Oscillator

Part Number: TUSB9261
Other Parts Discussed in Thread: TUSB9260,

After looking over both the TUSB9260 and TUSB9261 documentation and some posts on these forums I have two questions.

Even though the TUSB9261 doesn't require an external 1.8v supply, do you still need to use a 1.8v XO?

Can you use a 20MHz XO with the TUSB9261, or is it still recommended to only use a 40MHz XO?

Thanks!