Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848M: General question on PHY magnetics traces layout

Part Number: DP83848M

The question is general on PHY  magnetic layout:
Ideally the magnetics of the Ethernet is embedded in the RJ45.
However in my design, the magnetics must be on board. Furthermore the signals on the secondary of the transformer, that includes common mode choke pass through connectors and motherboard. Total of ~10 Iches.
My question is what is the recommended way to rout the traces  reference plain  up until they reach to the product Ethernet connector(which is not RJ45):
1)   Marinating 100 ohm using chassis ground as reference
2)   Passing the traces without reference ground and actually clearing any plane under the traces. (that would be difficult to do along all the race path)
3)   Using digital ground as the reference plane of the secondary traces. (In which I  believe is wrong to do)
Thanks

Avner