This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65981: Legacy USB-A device Configuration

Part Number: TPS65981
Other Parts Discussed in Thread: , HD3SS3212, HD3SS460

Hi,

We have our TPS65981 make boards and flashed our application image. Our application has to work with USB-C and Legacy USB-A data ports.

I made an application image which works well with USB-C data ports (Ex: Google Pixel Phone). The USB2.0 and USB3.0 data path in the board are terminated on the right side of the USB-C connector.

However, it is not working with USB-A ports devices (say nominal USB-A laptops). The processor USB2.0 data path is not terminated on the USB-C connector and USB3.0 SS data path is always connected to Group-1 of the USB-C connector. I guess I'm missing out few configurations in the application. Below I have attached our application image which works well on USB-C ports FYR. Could you provide me appropriate configuration setting for working with USB-A port devices?

TIIU_MMB1 TPS65981 HD3SS460 UFP Only 20171204.pjt

Thanks.