Part Number: HD3SS3220
1. In the data sheet it states : AC Coupling Capacitors for SS signals : 75-200 nF range allowed. For TX pairs only.
How do I choose the values of these capacitors ?
2. In the data sheet it states : AC Coupling Capacitors for SS signals : RX pairs will be biased by host Receiver. Note that HD3SS3220 requires a common mode biasing of 0-2 V. If host receiver has bias voltage outside this range, appropriate additional ac coupling caps and biasing of HD3SS3220 RX pairs needed
I will be implementing the HD3SS3220 into my peripheral device that is meant to be plugged into a regular PC or Laptop. How I am meant to know "If host receiver has bias voltage outside this range"
3. Why on the HD3SS3220 development board are there 0 ohm resistors (R19, R20, R21 & R23)