This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84-Q1: Delay time of LVDS output

Part Number: SN65DSI84-Q1

Hi,

Let me confirm about below.

According to datasheet, there is following spec for delay time of LVDS output.

According to this spec, condition is defined as "tc = 6.49ns(154MHz) and using REFCLK".

Then, I have following questions.

1. Even if user do not use "REFCLK", can we apply this spec as well ?

2. Is "Delay time" dependent on the frequency of LVDS clock ?

In datasheet condtion, LVDS Clock is 154MHz, but we would like you to confirm whether we can use this value for other LVDS clock case or not.

Best Regards,