Part Number: TPS65981
Hi, I am configuring the firmware for a TPS65981 using the Application Customization Tool v3.10. I have two questions regarding the I2C address in "General Settings"
1) As I understand, the TPS65981 only has one I2C port, yet two I2C addresses are shown in the Addressing field. Is the address labeled "Port1 I2C2" the correct address?
2) The effect of the DBG_CTL1 and DBG_CTL2 dropdowns seem to be reveresed to me. For example, I would expect a selection of "10" to reflect in an address of 0x2F and a selection of "01" to show 0x37, but the opposite is true. Are the dropdown labels wrong? Or is the calculated address wrong?
Thanks!