This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964-Q1: TESTEN Pin

Part Number: DS90UB964-Q1

[ DS90UB964-Q1 ] TESTEN Pin

Hi,

I can see two different circuits for TESTEN pin in the schematics of user's guide.
One is that TESTEN pin tied to GND directly, the other one is via 10kohm resistor.
I do believe that this can be connected to GND directly. Correct?



Thanks,
Ken