Other Parts Discussed in Thread: TPS2553D, TPS2069
Hi, Support team
When the capacitive load is connected on VBUS, the inrush current flows through the internal FET switch.
In this case, does TPS2069D quickly turn off the internal FET switch?
If it turns off, are there any delay timer to turn on the FET again?
As far as I see the bloack diagram of TPS2069D and TPS2553D, the operating function and processing of both devices is almost same, without reverse voltage protection , output discharge function and the point of current sensing.
Are there anything else as the difference?
Thanks
Tamio