Part Number: TUSB212
Is there any issue with connecting the RSTN pins on multiple TUSB212 devices, each with a 100nF cap at the pin, and driving the net with a single open-collector output? Obviously the RC timing on RSTN would be maintained with each TUSB212 having an internal 500K pull-up and a local 100nF cap. Is there any concern of the TUSB212 interfering with each other via the RSTN pins?