Part Number: SN65HVD82
Other Parts Discussed in Thread: SN65HVD96, TIDA-00527, SN65HVD78, THVD1550
Hi,
One of my application is to transmit Data and Power using 2 wires only. we have identified SN65HVD75DR or SN65HVD82DR or SN65HVD96 for this. kindly support for below queries.
1. Which IC is better, SN65HVD75DR or SN65HVD82DR or SN65HVD96?
2. How much voltage and current can be generated?
3. Will it be sufficient to drive another controller for displaying?
4. Will it generate power continuously or only during data transmission?
5. Will it work with standard modbus protocol or any other format/technique required to be followed?
| Which Series of IC is better, SN65HVD75DR or SN65HVD82DR or SN65HVD96? |
| How much voltage and current can be generated? |
| Will it be sufficient to drive another controller for displaying? |
| Will it generate power continuously or only during data transmission? |
| Will it work with standard modbus protocol or any other format/technique required to be followed? |
| OR |
| Data transmission using basic serial communication. Like UART? |