Other Parts Discussed in Thread: DS90UB913A-Q1
Now we can read and write the registers of the ds90ub964 through I2C.
Question:
In our design,we use DS90UB964-Q1 in our board ,and DS90UB913A-Q1 in camera, I configure the ds90ub964 based on the "1.10.10.1 Initialization" in Page 22 of 《DS90UB96X-Q1EVM User's Guide--Literature Number: SNLU177 July 2016》,the only difference is that the 0x6D register is set in the STP mode instead of the COAX mode(Because we're using the STP).After I configure the ds90ub964 as above,the 0x5B register was supposed to contain the Remote Serializer ID, but when I read the 0x5B register, I can not get the Remote Serializer ID,that is to say, ds90ub964 can not match with Remote Serializer.
I want to know that if I configure the ds90ub964 according to User's Guide in Page 22 step by step, is it enough to completely configure the ds90ub964 so that I can read the Camera ID and other informations?
If not, what other registers should I configure? thanks