Part Number: TL16C752C
Hi all
Would you mind if we ask TL16C752C?
<Question1>
On the datasheet P31, there is the description "IRQ Enable 0" on the MCR register bit3.
Does it mean that this register indicates IRQ Enable and default status is "0"?
<Question2>
On the datasheet P36, there is the description as follows;
0 = Forces the IRQ(A-B) outputs to high-impedance state
1 = Forces the IRQ(A-B) outputs to the active state
In loopback controls MSR[7]
Just in case, we would like to confirm one point.
About 1 = Forces the IRQ(A-B) outputs to the active state, does "the active state" mean Enable, right?
Kind regards,
Hirotaka Matsumoto