Part Number: TPS2543
Other Parts Discussed in Thread: TMS320F28069
Hi,
Application: (Single USB Port on a Embedded System)
1. User will Use to Charge Mobile (5V @ 1Amps) from this Embedded System.
2. Developer will use to store data in Pen drive from this Embedded System .
Below is the Schematic:
Doubts:
1. Is CDP Mode Choosen, correct for this application.
2. Hardwiring Ctrl 1, Ctrl 2, Ctrl 3, I_Lim_select Pins is Correct (?) (Pin 6,7,8,4)
3. As Enable Pin is also hardwired, Can status and fault pins left unconnected?
Regards,
Siddharth Gupta