Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB212: TUSB212 increases D +/- jitter more than TUSB211.

Guru 11170 points

Part Number: TUSB212
Other Parts Discussed in Thread: TUSB211

Hello E2E,

I compared TUSB211 and TUSB212 on same board and around .
I found that TUSB212 increases D +/- jitter more than TUSB211.
Please let me know the cause and solution.

Regards,
ACGUY

  • Please let me know the expert point of view.
  • ACGUY

    The jitter performance of TUSB212 should be the same as TUSB211. Are you using the same board for the comparison and how much jitter delta are you seeing between TUSB211 and TUSB212? It would be good if you can share your test result and schematic.

    Have you also tried to tune the EQ? Jitter caused by ISI could increase if the channel is not properly equalized.

    Thanks

    David

  • Hello David,

    Thank you for your reply.

    Measured results are as follow;
    Cable Length : 5m
    TUSB211(EQ-Level 3)
    - Signal rate : 479.9635Mbps (max : 552.74Mbps / min : 407.06Mbps)
    TUSB212(EQ-Level 2)
    - Signal rate : 480.0354Mbps (max : 577.14Mbps / min : 382.86Mbps)
    On same board.(Testing board)

    Regards,
    ACGUY
  • ACGUY

    This is signal rate, multiple components, such as clock frequency ppm, ISI from board channel, etc would affect it, It's not just jitter. You also need to use same EQ setting when doing comparison between TUSB211 and TUSB212.

    Thanks
    David