Other Parts Discussed in Thread: ISO3082, ISO3088
Hello All
We have made the circuit for RS485 to RS485 isolation using ISO3082. This circuit is working perfactly ok at baud rate of 38.4K. I have also checked at 187K & some times interface is failing. So we have replaced the ISO3082 with ISO3088 as it has higher speed. But this circuit is not working even at 9600 baudrate..
Pls. guide us for the same.
Thanks
mitesh