Part Number: TCAN1042-Q1
Hello Team,
I want to know the temperature characteristic of UVvcc(Falling undervoltage).
When Ta is high, the threshold becomes high? or low?
When Ta is low, the threshold becomes high? or low?
I would like to know the temperature condition that may be 4.25V(max).
> 7.6 Electrical Characteristics
> UVvcc(Falling undervoltage) 3.8~4.25V(-55℃~125℃)
If the threshold is high when Ta is high, please tell me if there is information on Typical value at 85℃/105℃.
Please give me an approximate value instead of a guaranteed value.
Best regards,
Kato