This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848K: reserved pin (pin: 8, 9, 10)

Guru 29720 points

Part Number: DP83848K

Hi Team,

I would like to confirm if reserved pin (pin: 8,9,10) are internally connected to the device or not.
The background of the question is my customer is evaluating DP83848K but they set these pins to be pull-up to VCC(=3.3V) through 2.2kΩ, so I would like to know the impact for their evaluation.

Best Regards,
Yaita / Japan disty