Part Number: TPS2553
Hi
My Customer has question.
Customers want to use the following specifications
VIN 1: 5.0 V
VIN 2: 3.3 V
※ Use exclusively by using the EN terminal. Please watch the attached file.
■Switching from 5 V to 3.3 V
In my opinion, if EN = OFF,
I do not think that there is no problem because it does not reverse flow.
■Switching 3.3 V to 5.0 V
In my opinion, reverse flow protection works at switching timing, and
I think there is a possibility that the device will shutdown.
Is this idea correct?
Regard
T Kishi