Part Number: DP83822H
The datasheet of the DP83822H says "A 4.87 kΩ +/-1% resistor must be connected from RBIAS to GND."
In your "DP83822 EVM Getting Started" you use a thik film resistor (CRCW04024K87FKED) wich has a tolerance of 1% but a stability of deltaR/R = 1 % for 1000 h at 70 ° C and 100ppm temperatur tolerance. So the overall tolerance is much more than 1%.
I want to know wich overall tolerance for the bias resistor is needed. 1% can not be the answer.